Debug features#
SimpleSwitch™ debug features of the package can be enabled using the --debug
parameter. So far the only debug feature enabled in this mode is
Live update in QEMU,
exporting package filesystem over NFS during runtime.
Note
The debug features do not enable software debugging tools such as GDB. Using these tools can be controlled through the startup command.