- ...
- SDK
- Yocto
- ...
- ...
- tools
- debug
- package
- deploy
- debug
Bind mount#
It is possible to create some bind mounts between the host and a SimpleSwitch™
package using the parameters --bind-src-path and -bind-dst-path. The
first one is used to define the path on the host, and the second one to define
the path in the SimpleSwitch™ package. These parameters can be used multiple
times to create multiple bind mounts. They must be provided in equal number,
as one --bind-src-path is linked to one -bind-dst-path in the order
they are parsed.