- ...
- SDK
- Yocto
- ...
- ...
- your first application
- tools
- ...
Getting started with C/C++#
If you want to create a SimpleSwitch™ application using C/C++, please follow this guide to get you easily started.
Example Project#
Here is a very small C project, with a single C source file, test.c:
// SPDX-FileCopyrightText: (C) 2025 Tria Techonologies GmbH
// SPDX-License-Identifier: LicenseRef-Avnet-OSS-1.0
#include <stdio.h>
#include <unistd.h>
int main()
{
while(1) {
fprintf(stderr, "Test C SDK\n");
sleep(5);
}
return 0;
}
And a Makefile:
# SPDX-FileCopyrightText: (C) 2022 Avnet Embedded GmbH
# SPDX-License-Identifier: LicenseRef-Avnet-OSS-1.0
BIN = c_test_prog
OBJS = test.o
PREFIX ?= ""
all: $(BIN)
$(BIN): $(OBJS)
$(CC) -o $@ $<
clean:
rm -f $(BIN) $(OBJS)
install: $(BIN)
install -m 0755 -d "$(PREFIX)/opt/$(BIN)"
install -m 0755 $(BIN) "$(PREFIX)/opt/$(BIN)"
.PHONY: clean install
One can build this project for the host system by putting both file in the same
directory and running make
make
./c_test_prog
Test C SDK
Build the project using a Makefile#
With a makefile aware of cross-compilation, building the binary is as simple as
sourcing the SDK (see Source the SDK) and running make, e.g.
make
If the makefile has an install target using the PREFIX variable as
installation path, it can be used directly with the --makefile-dir option of
the Generate a SimpleSwitch™ package script
simpleswitch-generate-package --name simpleswitch-example --makefile-dir . \
--template C --startup-command /opt/c_test_prog/c_test_prog
Or if you want to be able to debug your application:
simpleswitch-generate-package --name simpleswitch-example --makefile-dir . \
--template C --startup-command "while true; do gdbserver :2159 /opt/c_test_prog/c_test_prog ; done"
If your makefile lack of a compatible install target, see below.
Deploy to the target#
Now it is time to deploy the generated SimpleSwitch™ container to the device. For this please see Deploy a SimpleSwitch™ package
Remote debugging a C/C++ application#
To remote debugging a C or a C++ application, you can see Remote debug a SimpleSwitch™ package
Further reading#
See also