I cannot connect the device to my network#

If you can’t connect the device to your network, we can still bringup a local network between the device and your computer.

Please see our simpleswitch-dhcp-helper, that is already pre-installed into the base image.

Tip

If you don’t have a serial terminal available, you can as well use our SimpleSwitch™-launcher

To allow internet access of the connected device please see our guide at Access GHCR from a private network with no direct access to internet