Create your own DISTRO based on SimpleCore™#
After you are done with Create a project specific layer you can define your own Distribution.
This is especially helpful, if you want to change the used logo. See Custom Logos and branding for more details.
Create a distro config#
Browse to the root path of your project layer and run
mkdir -p conf/distro
touch conf/distro/mydistro.conf
and fill the new file mydistro.conf with the following content
require conf/distro/simplecore-distro.conf
you can now add more settings below that line.
Start your build#
from the console you can now run
DISTRO="mydistro" bitbake <image>
DISTRO="mydistro" scotty build <image>