• ...
  • Yocto
  • production
  • project creation
  • SDK extension
  • SimpleSwitch
  • packages
  • images

SIMPLESWITCH_STARTUP_COMMAND#

SIMPLESWITCH_STARTUP_COMMAND = "/usr/bin/app"

defines what program, script or service will be called when the SimpleSwitch™ package is started.

Tip

If you have a more complex startup sequence it is advised to put it into a separate shell script, which then can be set as SIMPLESWITCH_STARTUP_COMMAND

Do not use in combination with SIMPLESWITCH_CONFIGURE_STARTUP

using SIMPLESWITCH_CONFIGURE_STARTUP will overwrite any settings made to this variable

See also