- ...
- Yocto
- production
- project creation
- SDK extension
- SimpleSwitch
- packages
- images
SIMPLESWITCH_DEPENDENCIES#
Dependencies to add in the manifest can be described directly in the Yocto
recipe with the SIMPLESWITCH_DEPENDENCIES variable
SIMPLESWITCH_DEPENDENCIES = "simpleswitch-application-1 simpleswitch-application-2"
See also
in the SimpleSwitch™ manifest: Depend on other SimpleSwitch™ packages
from the SDK: Package dependencies