Flashing from SDcard/USB stick to eMMC#
You can flash the content of a SDCard/USB stick to the eMMC of the device
boot up the device
login into the shell (default
root, no password)run
distro-installer
The installation will now replicate the SDCard/USB stick onto the eMMC, including all files and settings.
This could, depending on the size of the SDCard/USB stick take a moment.
Once finished with Image successfully installed onto /dev/mmcblk2 you can change the
boot options on your EP1/EP5 and boot up the same system from eMMC.
Note
During the installation, paths in /etc/ are changed from the old
boot medium to eMMC paths.
If you have configuration outside of this path that refers to hardcoded
paths to /dev/mmcblk, these need to be adjusted. It is possible to
do it manually or to set the SIMPLECORE_DISTRO_INSTALLER_HOOK variable
in the distro-installer recipe to run some extra shell commands.