- ...
- SDK
- Yocto
- ...
- ...
- tools
- debug
- package
- deploy
- debug
Generate a SimpleSwitch™ package#
The simpleswitch-generate-package script helps to create SimpleSwitch™
packages from existing templates, without requiring to use Yocto. It will merge
the template files and your own file to generate a SimpleSwitch™ package and its
manifest fragment.
SimpleSwitch™ Package Creation Example#
Copying your own files over the SimpleSwitch™ template can be done using the following command
simpleswitch-generate-package --name simpleswitch-example --copy-dir deploy_dir \
--template c --startup-command /usr/bin/c_test_prog
- This will generate two files:
simpleswitch-example.ext4: A filesystem containing the merge of the template and your files. It needs to be deployed in the/appsfolder of the target.simpleswitch-example.simpleswitchpackage: A fragment of SimpleSwitch™ manifest. It needs to be concatenated to the/apps/simpleswitch-manifest.yamlfile on the target.
Directory deploy_dir must contain all files to copy in the package, in a
structure reflecting its hierarchy in the package
find deploy_dir -printf "%y %p\n"
d deploy_dir
d deploy_dir/usr
d deploy_dir/usr/bin
f deploy_dir/usr/bin/c_test_prog
template can be changed according to the desired template, run
simpleswitch-generate-package --help to list all supported templates.
Finally, the startup command is specified using the --startup-command
parameter.
Advanced usage#
Detailed usage of simpleswitch-generate-package#
simpleswitch-generate-package --help
Usage: simpleswitch-generate-package
Options:
-n|--name package # Set the output package name.
-S|--size size # Set the output filesystem size in kilobytes (default: automatic).
--size-factor # Set the factor used to compute automatic filesystem size (default: 1.2).
-c|--copy-dir directory[:destination_prefix] # Add a directory to recursively copy in package.
-m|--makefile-dir directory # Add a directory in which to run 'make install'.
-s|--startup-command command # Set the command to run on application start.
-I|--install-command command # Set the command to run on package installation.
-U|--uninstall-command command # Set the command to run on package removal.
-t|--template # Set the template package to use (possible values: python,qt,c,flutter).
-d|--debug # Start the container in debug mode.
-D|--depends-on # Set the package dependencies.
-u|--allow-update # Allow to reuse files from the previous build.
-w|--work-dir # Set the output directory.
-p|--storage-size # Set the size of the persistent container storage in bytes.
-a|--bind-src-path # Add a source path for a bind mount. This option can be repeated.
-b|--bind-dst-path # Add a destination path for a bind mount. This option can be repeated.
-N|--no-autostart # Disable the autostart of the app.