- ...
- Yocto
- production
- project creation
- SDK extension
- SimpleSwitch
- packages
- images
SIMPLESWITCH_UNINSTALL_COMMAND#
SIMPLESWITCH_UNINSTALL_COMMAND = "/usr/bin/uninstall-script"
defines what program, script or service will be called when the SimpleSwitch™ package is uninstalled.
That can be used to remove/undo changes by the container to e.g. /apps.
Tip
If you have a more complex startup sequence it is advised to put it into a separate
shell script, which then can be set as SIMPLESWITCH_UNINSTALL_COMMAND
See also
from the SDK: Generate a SimpleSwitch™ package