- ...
- Yocto
- production
- project creation
- SDK extension
- SimpleSwitch
- packages
- images
SimpleSwitch™ docker package#
To ensure that there will no conflicts between the docker image and the assembled Yocto image, we will have to add
inherit simpleswitch-dockerpackage
to the image recipe instead of
inherit simpleswitch-package
This will provide a safe baseline to create the final container image.
Here be dragons
Installation of multiple
dockerimagebased recipes in onesimpleswitch-docker-package, will likely create conflicts between different files and folders.