- ...
- Yocto
- production
- project creation
- SDK extension
- SimpleSwitch
- packages
- images
SIMPLESWITCH_INSTALL_COMMAND#
SIMPLESWITCH_INSTALL_COMMAND = "/usr/bin/install-script"
defines what program, script or service will be called when the SimpleSwitch™ package is installed.
That can be used to install e.g. configuration files to /apps that should be accessible to the user.
Tip
If you have a more complex startup sequence it is advised to put it into a separate
shell script, which then can be set as SIMPLESWITCH_INSTALL_COMMAND
See also
from the SDK: Generate a SimpleSwitch™ package