freeze#
usage: scotty freeze [-h] basepath files [files ...]
Freeze a configuration file
positional arguments:
basepath Base directory to store the files to
files Files to freeze
options:
-h, --help show this help message and exit
freeze command will turn any loose revision information of git repositories used in the
current kas based configuration into
fixed SHA256 based revisions.
This can be used e.g. to create a release.
Note
For every file that is affected a overlay will be created under the configured basepath.
Those new files should then be put under version control (e.g. git).
You can request scotty to use these files with --manifest-overlays-from option or
with the help of SCOTTY_MANIFEST_OVERLAYS environment variable.
example:
Check out e.g. simplecore-manifest directory.
$ cd <path to simplecore-manifest>
$ scotty freeze release $(find snippets -name '*.yml' | tr "\n" " ")
the newly created files can now be committed to git
To use these frozen revisions run
$ cd <path to simplecore-manifest>
$ scotty --manifest-overlays-from "release" setup
or
$ cd <path to simplecore-manifest>
$ SCOTTY_MANIFEST_OVERLAYS="release" scotty setup