- ...
- SDK
- Yocto
- ...
- ...
- your first application
- tools
- ...
Getting started with Python#
Before you start#
Before we can use the SimpleSwitch™ SDK for Python we need to download the SDK extension. For this you need to run from the sourced SimpleSwitch™ SDK
GITHUB_TOKEN="<your personal access token for Github>" GITHUB_USERNAME="<your Github username>" simpleswitch-sdk-tool install python
eval "$(simpleswitch-sdk-tool activate)"
Github personal access token
To create a Github personal access token see Github container registry (GHCR)
Start a Python project#
Recommended directory structure#
All python source files should be placed into a folder called src.
Example Python Project#
Here is a very small Python project, with a single Python source file, src/app.py:
#!/usr/bin/env python3
# SPDX-FileCopyrightText: (C) 2022 Avnet Embedded GmbH
# SPDX-License-Identifier: LicenseRef-Avnet-OSS-1.0
"""Python test."""
import logging
import time
if __name__ == "__main__":
while True:
logging.warning("Python test ok")
time.sleep(5)
Build the Python project#
First source the SDK (see Source the SDK)
Using simpleswitch-generate-package with Python#
You can also create a package by copying the content of a directory. All you need is this directory to reproduce the structure desired in the package. For this we need to create a Linux root file system like structure like
find deploy_dir -printf "%y %p\n"
d deploy_dir
d deploy_dir/usr
d deploy_dir/usr/bin
f deploy_dir/usr/bin/app.py
In case the directory doesn’t exist yet run
mkdir -p deploy_dir/usr/bin
Then copy the Python script and give it execution rights
cp src/app.py deploy_dir/usr/bin
chmod +x deploy_dir/usr/bin/app.py
You can then use the --copy-dir option of the
simpleswitch-generate-package the Generate a SimpleSwitch™ package script
simpleswitch-generate-package --name simpleswitch-example --copy-dir deploy_dir \
--template python --startup-command /usr/bin/app.py
Or if you want to create a debuggable version run
simpleswitch-generate-package --name simpleswitch-example --copy-dir deploy_dir \
--template python --startup-command "/usr/bin/python3 -m debugpy --listen 0.0.0.0:5678 --wait-for-client /usr/bin/app.py"
Deploy to the target#
Now it is time to deploy the generated SimpleSwitch™ container to the device. For this please see Deploy a SimpleSwitch™ package
Remote debugging a Python application#
For debugging python we are using the Debug Adapter Protocol which is also supported by several other tools.
Further reading#
See also