- ...
- Yocto
- production
- project creation
- SDK extension
- SimpleSwitch
- packages
- images
SIMPLESWITCH_CONFIGURE_CONFIG#
SIMPLESWITCH_CONFIGURE_CONFIG = "/usr/data/some/path/config.json"
will allow to set the path of the default configuration, when using Dynamically configure SimpleSwitch™ packages.
The default is /apps/${SIMPLESWITCH_PACKAGE_NAME}/config.json
See also
from the SDK: Generate a SimpleSwitch™ package