- ...
- Yocto
- production
- project creation
- SDK extension
- SimpleSwitch
- packages
- images
SimpleSwitch™ out of docker containers#
By adding
inherit dockerimage
SRC_URI = "docker://<image>;sha256sum=<checksum>"
to every recipe we can download an image from docker hub and reuse it as a SimpleSwitch™ image.
Example#
SRC_URI = "docker://filebrowser/filebrowser;arch=${ARCH};version=v${PV};sha256sum=${CHECKSUM}"
inherit dockerimage
ARCH = "doesnot-exist"
ARCH:sm2s-imx8-all = "arm64"
ARCH:sm2s-intel-all = "amd64"
CHECKSUM = "nochecksum"
CHECKSUM:sm2s-imx8-all = "e5e4444948c3b93cf6c647dee58590f30f76838170470851414a4b271a07ffad"
CHECKSUM:sm2s-intel-all = "4478da6483e6050dbf0c5f6c6b3206b9d9a7984ba8180fc94b83d667fee51815"
will download filebrowser for the correct architecture of your build.
Note
ARCHneeds to be set for all supported SOMs specifically, check theOS/ARCHtab on the Docker Hub to find the best match.CHECKSUMneeds to be set to the SHA256 checksum calculated by the bitbake build system. Best is it to build with a wrong checksum and get the correct one from the build output of bitbake.
Options explained#
Here be dragons
Do not use
latesttags on images, as they can change at any point in time without further notice.Currently we don’t support the creation of SimpleSwitch™ packages out of private registries.
SBOM/licensing of the recipe will inevitably not reflect all of the software used in the container.
Installation of multiple
dockerimagebased recipes in onesimpleswitch-docker-package, will likely create conflicts between different files and folders.the implementation will fail if
hub.docker.comdoes not offer an image for Linux and your target architecture.devtool integration does not work with an out of tree fetcher
devtool check-upgrade-statuscan be emulated by runningbitbake <recipe> -c do_check_upgrade_statusresp.scotty bitbake <recipe> -c do_check_upgrade_status