i.MX8 SOCs#
The images can be found at
sm2s-imx8plus eMMC image:
build/build/tmp/deploy/images/sm2s-imx8plus/simplecore-weston-demo-image-sm2s-imx8plus.wicsm2s-imx8plus bootloader+SPL:
build/build/tmp/deploy/images/sm2s-imx8plus/imx-boot-sm2s-imx8plus-sd.bin-flash_hdmi_spl_ubootsm2s-imx8mini eMMC image:
build/build/tmp/deploy/images/sm2s-imx8mini/simplecore-weston-demo-image-sm2s-imx8mini.wicsm2s-imx8mini bootloader+SPL:
build/build/tmp/deploy/images/sm2s-imx8mini/imx-boot-sm2s-imx8mini-sd.bin-flash_hdmi_spl_ubootsm2s-imx8nano eMMC image:
build/build/tmp/deploy/images/sm2s-imx8nano/simplecore-weston-demo-image-sm2s-imx8nano.wicsm2s-imx8nano bootloader+SPL:
build/build/tmp/deploy/images/sm2s-imx8nano/imx-boot-sm2s-imx8nano-sd.bin-flash_ddr4_evk
After flashing succeeded and a reset is performed the board will boot up and a Weston UI is shown. You can also access the device via RS232 serial port.
The following ways are possible:
We advise for Flash using Etcher or Flash using bmaptool.
Flashing just the bootloader on i.MX8 SOCs#
To just flash the bootloader from the SDCard/USB stick, run
/boot/emmc_boot0_install.sh
/boot/emmc_boot1_install.sh
This option is not available on other platforms.