- ...
- Yocto
- production
- project creation
- SDK extension
- SimpleSwitch
- packages
- images
SIMPLESWITCH_BIND_MOUNTS#
The variable SIMPLESWITCH_BIND_MOUNTS is here to create some bind mounts
between the host and the SimpleSwitch™ container. A bind mount is described by
the source path on the host and the destination path on the SimpleSwitch™
package separated by :. It is possible to create multiple bind mounts
separating them by a space. If the source path belong the apps partition
the Wic tool will create the directory automatically. If it is not the case
it is the responsibility of the user to create the directory before the
SimpleSwitch™ application start.
Example
SIMPLESWITCH_BIND_MOUNTS = "/apps/my-data:/usr/share/my-data /tmp/other-data:/tmp/other-data"
See also
from the SDK: Bind mount