Setup your workspace#

Setting-up Serial Debug (all SOM)#

To get a serial debug console, make sure to connect the serial debug cable as documented in the Tria User Manual for your main board and use your preferred serial terminal. Here is an example with picocom

$ picocom -b 115200 /dev/ttyUSB0

Setting up the serial console can also be done via minicom. Create a file in /etc/minicom/ named minirc.<console-name>, e.g. minirc.serial-imx8plus with the following content

# Machine-generated file - use "minicom -s" to change parameters.
pu port             /dev/ttyUSB0
pu baudrate         115200
pu bits             8
pu parity           N
pu stopbits         1
pu linewrap         Yes
pu addcarreturn     Yes
pu rtscts           No

And then, to run it

$ minicom serial-imx8plus

Setting-up Serial Debug (QEMU)#

To get a serial debug console, if running with libvirt, run the following command

$ virsh -c qemu:///system console ${VM_NAME}