The Scotty tool#
Scotty#
SimpleCore™ open technology tool for you or short Scotty is a tool used to
operate with the SimpleCore™ BSP, helping to download sources and build BSP images. It
relies on docker to provide a reproducible build environment.
Scotty can either be used as a single command to build a full image or as a
helper to setup Yocto sources and open a shell with a Yocto environment.
Getting started#
The scotty tool relies on a docker container to embed as much as possible the software dependencies it relies on. As a consequence, you will need to make sure to install Docker<https://www.docker.com/> on your system and make sure your user has rights to use docker. The scotty tool also needs OpenSSL<https://www.openssl.org/> to function properly.
On Ubuntu 20.04 platforms, they can be installed with following commands:
$ sudo apt install docker.io openssl
$ sudo gpasswd -a ${USER} docker
In addition, if you plan to use QEMU images, it is advised to make sure the
current user is able to use KVM,
having write permissions to /dev/kvm. On Ubuntu 20.04, this can be done by
adding your user to the kvm group, with the following command:
$ sudo gpasswd -a ${USER} kvm
Note
After adding your user to the docker or kvm group with the gpasswd
command, you will need to open a new session to apply your new privileges.
Installing the scotty tool can be easily done with pip
pip install --user avnet-scotty
upgrading an existing installation can be done with
pip install --user --upgrade avnet-scotty
Important
On Ubuntu 20.04 you might be affected by this bug,
so ${HOME}/.local/bin is not part of the standard search path.
This can be fixed by running
echo 'export PATH="$(systemd-path user-binaries):$PATH"' >> ~/.bashrc
Note
A reboot is required for the setting to become effective.
You can also install scotty with
sudo pip install avnet-scotty
but that requires you to have sudo rights on your system.
Alternatively, the current development version can be obtained by cloning avnet-embedded/simplecore-tools.
Potential pitfall
If you are facing the following issue
Error response from daemon: Head "https://ghcr.io/v2/avnet-embedded/scotty/manifests/2023.10": denied: denied
scotty failed on line 157
please run
docker logout ghcr.io
on your computer.
To fix it permantely, please create a personal access token, as described at Github container registry (GHCR)
with at least read:packages permissions.
And re-login to docker using
docker login ghcr.io
Github preparations#
Before we can start to build, we need to make sure that Github allows us to connect via ssh.
See this video on how to do it
Please also keep in mind that most of the repositories are only available for users being part of avnet-embedded GitHub organization.
Please reach out to support to request access.
Running scotty on a different docker image#
By default scotty will use the corresponding version of the scotty docker image. To use a different docker image run:
$ SCOTTY_DOCKER_IMAGE=<image> scotty ...
e.g. to use the latest development version:
$ SCOTTY_DOCKER_IMAGE="ghcr.io/avnet-embedded/simplecore-tools:kirkstone" scotty ...
to use a different release:
$ SCOTTY_DOCKER_IMAGE="ghcr.io/avnet-embedded/scotty:<release tag>" scotty ...
Scotty subcommands#
- Several commands are supported by Scotty, with different goals:
update: download or update the Yocto sources. Will be triggered implicitly with default parameters if no sources are found.setup: Setup the build directory. Will be triggered implicitly with default parameters if the build directory has not been setup.bitbake: Build a Yocto target.shell: Run a shell in the Yocto build environment.command: Run a command in the Yocto build environment.docker-update: Update Scotty build container.info: Print out information.
Setup your build#
With
$ scotty setup
you can configure your build through our interactive UI.
Note
$ scotty setup --force
Will allow you to redo the configuration at any point.
Building a full image#
A single command is enough to download the sources and build an image:
$ scotty bitbake core-image-minimal
Built images can then be found in build/build/tmp/deploy/images/.
The build target can be customized:
$ scotty bitbake core-image-minimal
$ scotty bitbake -- core-image-minimal -c populate_sdk
Note
The available images/SDKs can be displayed by running
$ scotty info images
Recommended hardware setup#
For building software pacakges with Scotty we recommend the following minimal hardware setup:
For base images
4 Cores / 8 threads CPU
16GB RAM
200GB HDD
For SDKs
16 Cores / 32 threads CPU
64Gb RAM
500GB HDD
Note
Other combinations do work as well, but keep in mind that we at least require 2GB of RAM per available CPU thread.
Using Scotty as a helper#
Scotty can be used to open a shell with a sourced Yocto environment:
$ scotty shell
It can also be used to run a single command without opening a shell:
# This is equivalent to scotty bitbake core-image-minimal
$ scotty command bitbake core-image-minimal
$ scotty command bitbake-layers show-appends
Updating sources#
Scotty will not modify downloaded sources by itself after the initial setup. Building an image with up-to-date sources can be done using following commands:
$ scotty update
$ scotty bitbake core-image-minimal
Advanced configuration#
Scotty can be used to download extra sources, add additional layers or tweak the configuration.
Supported update arguments#
--manifest-branch: Set repo branch used for repo init.--manifest-url: Set repo url used for repo init.--manifest-name: Set repo manifest used for repo init.--extra-download: Add an extra git to download. If this is a layer, it can then be used in setup with--extra-layer.
Supported setup arguments#
--build-dir: Set build subdirectory, subdirectory ofbuild. Can be used to have different builds in the samebuildfolder.--machine-dir: specify the directories where scotty should look for supported machines.--extra-layer: Add an extra local layer.--extra-conf: Add an extra configuration entry in local.conf.--extra-env: Pass on additional environment variables.--sstate-mirrors: Do use any sstate mirror (default = false).--features-layers-set: The set of Tria extra layers to use.--machine-dir: specify the directories where scotty should look for supported machines.
Note
The currently available --features-layers-set can be displayed by running
$ scotty info feature-sets
Supported bitbake, shell and command arguments#
--build-dir: Set build subdirectory, subdirectory ofbuild. Can be used to have different builds in the samebuildfolder.
Scripting configuration#
It might be useful to skip the configuration menu, so Scotty can be used in a scripted way. To help with this, most configuration can be set either through arguments or environment variables.
Supported arguments#
The --features-layers-set of the setup subcommand can be used to bypass
layer sets selection.
Supported environment variables#
DISTRO: Can be used to select the Yocto distro and skip selection menu.MACHINE: Can be used to select the Yocto machine and skip selection menu.ACCEPT_FSL_EULA: Can be used to set the Freescale/NXP EULA status and skip selection menu if applicable).LICENSE_FLAGS_ACCEPTED: Can be use to allow e.g. commercial licenses in the resulting images.UBOOT_ENV_VARS: Can be use to prepopulate the used u-boot environment (expects a key value list, separated by new lines). To disable pass “ “.SCOTTY_FEATURE_LAYERS: A space separated list of feature layers (alternative toscotty setup --features-layers-set- CLI flags have always precedence).
Example#
$ export ACCEPT_FSL_EULA=1
$ export LICENSE_FLAGS_ACCEPTED=commercial
$ DISTRO=simplecore-distro MACHINE=sm2s-imx8plus scotty setup --features-layers-set distro
$ scotty bitbake core-image-minimal
In addition, it is possible to tweak Scotty behaviour using the environment:
SCOTTY_ALLOWLIST: The list of host environment variables exposed in Yocto environment.DOCKER_EXTRA_ARGS: Additional parameters for docker.
Example
$ export DOCKER_EXTRA_ARGS="-v /home/downloads:/home/scotty/build/downloads -v /home/sstate-cache:/home/scotty/build/sstate-cache"
$ scotty bitbake core-image-minimal
Using Scotty on Windows#
Scotty has been tested on Windows with WSL2.
Installation#
The following will need Administator permission
enable and install
Windows subsystem for Linux 2like decribed here.We recommend to use the
Ubuntuvirtual machine for WSL2.NOTE only version 2 of WSL is supported.
install docker on WSL2
install
openssh
$ sudo apt update
$ sudo apt install openssh-server
install
pip
$ sudo apt update
$ sudo apt install -y python3-pip
and finally install scotty
$ pip3 install avnet-scotty
Configure WSL2#
It is recommended to disable the /etc/resolv.conf updating. For that run from within the WSL2 VM
$ echo "[network]" >> /etc/wsl.conf
$ echo "generateResolvConf = false" >> /etc/wsl.conf
now close the WSL2 VM window.
Dependending on the CPU count and the available RAM of your Windows machine you’ll need to configure the following:
From a cmd.exe on Windows
$ cd %userprofile%
$ notepad .wslconfig
Now add the following to the file
[wsl2]
processors=<Amount of RAM in GB / 4>
swap=<Free disk space in GB - 150>GB
so for a Windows PC with 16 cores, 16GB of RAM and 300GB of free disk space that would be
[wsl2]
processors=4
swap=150GB
save the file, close the window and run
$ wsl --shutdown
after that you can launch your WSL VM and start using scotty.
SSH keys#
For scotty to work properly you’ll need to create and reference SSH keys for Github, like
described on this page.
Reusing your SSH keys from Windows#
In case you want to reuse your SSH keys from windows just run
$ mkdir -p ~/.ssh
$ cp /mnt/c/Users/<your Windows username>/.ssh/* ~/.ssh/
$ chmod 0400 ~/.ssh/id_*
Using WSL2 with VSCode#
You’ll need to install this extension in your VSCode and configure it like shown on the website.
Using Scotty without Docker#
If needed, Scotty can be used without docker. In this case, you are in charge of
providing a fully configured environment. This can be done by setting the
SCOTTY_USE_DOCKER environment variable:
$ SCOTTY_USE_DOCKER=0 scotty bitbake core-image-minimal
Scotty Runqemu#
Scotty Runqemu is an additional tool allowing to start QEMU to run a QEMU targeted build.
Runqemu Example#
$ export DISTRO=simplecore-distro MACHINE=qemux86-64
$ scotty setup --features-layers-set examples
$ scotty bitbake simplecore-weston-demo-image
$ scotty-runqemu simplecore-weston-demo-image
Note
In case your machine does not offer KVM support run
$ SCOTTY_QEMUNOKVM=1 SCOTTY_ALLOWLIST="QEMU_USE_KVM" QEMU_USE_KVM=0 scotty-runqemu --extra-env=QEMU_USE_KVM simplecore-weston-demo-image
Note
In you like to start an image in headless mode (no graphics) run
$ SCOTTY_QEMUNOGPAHIC=1 scotty-runqemu simplecore-weston-demo-image
scotty-test#
scotty-test is a helper tool to run tests on real hardware.
It will guide the user through the needed steps and create a test report.
To run you will need
an Azure access token
SAS_TOKENaccess to simplecore-tools repository
a Github account
a computer running Linux -
sudo,dd,gitinstalled - your git client propely setupa SDCard
Internet access
the hardware you want to test
$ SAS_TOKEN=abcdef scotty-test
The tool will download the necessary images and SDKs, run the tests and create a Markdown report that will be pushed to the simplecore-tools repository.
Manual or Automatic tests#
The user can choose to run manual tests, meaning that all the tests will be run but some will need an interaction with the user. For example, the user will have to change switches or measure the pins’ voltage with a multimeter.
Otherwise if the user chooses automatic tests, it will run only the tests that do not need an interaction with the user. And for example, if there is a GPIO Expander connected, it will use it to check the voltage of the pins automatically.
Use Labgrid#
Labgrid is a tool for automated testing. It can be used to flash the SD Card used for the tests.
To run the tests with Labgrid the user will need:
a SDWireC
a serial connection to the board
a USB hub
It is then necessary to configure the exporter file corresponding to the machine in tools/labgrid/client/.
For the serial port, the SDWireC and the Numato GPIO Expander, it is possible to use this kind of command to get the ID_PATH:
$ udevadm info /dev/ttyUSB0
For the Tasmota Power, it is possible to get the topics names after seting it up using the manual.
Labgrid creates places for each board and associates to them a serial port, a SDWireC, a GPIO Expander and a Tasmota power plug. The user can check the places acquired by Labgrid at 172.17.0.2.
Labgrid flashes the image automatically thanks to the SDWireC and then gives the IP address of the board to scotty-test so it could run the tests.
scotty-layers.yaml#
All the information scotty uses is defined in scotty-layers.yaml in the manifest repository.
This file is a yaml file containing the following sections:
base section#
Allowed number of sections in the yaml: 1
This section defines the layers that are always used in any setup.
Key |
Type |
Description |
Example |
|---|---|---|---|
description |
string |
Human readable description |
description: “My base layers” |
layers |
list |
Paths to layers to be used |
|
licenses |
list |
additional EULA/licenses to be accepted by the user |
|
NOTE: licenses is optional
distro_* section#
Allowed number of sections in the yaml: 1..n
These sections define the possible selections for Yocto’s DISTRO setting.
Key |
Type |
Description |
Example |
|---|---|---|---|
description |
string |
Human readable description |
description: “Super Distro” |
menu_priority |
int |
Defines the order in the menu |
menu_priority: 100 |
layers |
list |
Paths to layers to be used |
|
supported_distros |
dict |
key/value table of DISTRO name and description |
|
machines_* section#
Allowed number of sections in the yaml: 1..n
These sections define the needed layer set for the selected MACHINE entry.
Key |
Type |
Description |
Example |
|---|---|---|---|
description |
string |
Human readable description |
description: “My machine layers” |
layers |
list |
Paths to layers to be used |
|
machine_pattern |
string |
Regular expression matching |
machine_pattern: “sm2s-.l” |
overlays_* section#
Allowed number of sections in the yaml: 0..n
These sections define the available device tree overlays to be selectable by scotty
Key |
Type |
Description |
Example |
|---|---|---|---|
description |
string |
Human readable description |
description: “My overlays” |
overlays |
dict |
|
|
machine_pattern |
string |
Regular expression matching |
machine_pattern: “sm2s-.l” |
feature_* section#
Allowed number of sections in the yaml: 0..n
These sections define the possible selections for additional features. Features can reference each other by using yaml anchors.
The following example
feature_myfeature:
menu_priority: 200
description: "My feature layer"
layers: &layers_myfeature
<<: [*layers_poky]
? "meta-myfeature"
supported_distros: &distros_myfeature
<<: [*distros_poky]
defines a feature that is called My feature layer. It will add meta-myfeature to the layer set, and is only applicable
if poky is selected as a DISTRO. By selecting this feature all layers defined by the poky DISTRO will be setup as well.
Key |
Type |
Description |
Example |
|---|---|---|---|
description |
string |
Human readable description |
description: “My feature” |
menu_priority |
int |
Defines the order in the menu |
menu_priority: 100 |
layers |
list |
Paths to layers to be used |
|
extraconf |
list |
Extra configuration variables for local.conf |
|
supported_distros |
dict |
key/value table of DISTRO name and description |
|
add-overlays |
object or list |
Additional selectable overlays of the feature see overlays section for details |
or
|
scotty-layers.ext.yaml#
scotty will additionally scan for scotty-layers.ext.yaml in the checked out repositories.
These files are written in the same syntax as scotty-layers.yaml and allow the standard scotty-layers.yaml to be extended.
The files have to be placed in the root of the bitbake layer.