Cog Browser Demo#
The simpleswitch-cog offers a demo of Cog Browser based on Webkit technology.
It will open the Tria Website in fullscreen mode.
Registration
If you want to test SimpleCore™, SimpleSwitch™ or any of our packages from our SimpleCore™ incubator program, please register here and we will grant you access.
Configure Cog#
To add startup settings to all browsers, edit /apps/browser/homepage.txt.
To add startup settings to Cog only, edit /apps/cog/homepage.txt.
The Cog configuration file takes precedence over the global browser configuration file.
Multiple settings can be specified as a multiline list, for example
https://www.google.com
--scale=0.1
--bg-color=FF0000
The lines can contain spaces.
However, neither use \ separators nor options as –option=’1 2 3’ (it should not happen as most cog options are switches or coma separated lists).
# can be used in an option free line to write license informations or comments.
- Settings example :
Add
https://www.learningcontainer.com/wp-content/uploads/2020/05/sample-ogv-file.ogvto show case video support.Specify the URL
Add
--scale=FACTORto set the zoom factor applied to web contentAdd
--doc-viewerto disable Cog’s resource cache (useful for systems with limited RAM)
See Cog command line options for an extended overview of the available settings:
cog -h
cog --help-all
How to get it#
## From the base image run
$ skopeo login ghcr.io
$ export machine=$CONTAINER_HELPER_ARCH
$ export package=simpleswitch-cog
$ export tag=$RELEASE_VERSION
$ container-helper registry-install ghcr.io ghcr.io/avnet-embedded/simpleswitch/${machine}/${package}:${tag}
$ simpleswitch-helper start ${package}
## On your computer run
$ scotty build simpleswitch-cog
## On your computer run
$ bitbake simpleswitch-cog
Note
This recipe needs meta-webkit in the layer setup, if you want to build it yourself.
## On your computer run
$ scotty setup --features-layers-set webkit --features-layers-set simpleswitch
## On your computer run
$ bitbake-layers add-layer <path to meta-webkit>