Fallback DHCP server#
simpleswitch-dhcp-helper offers a fallback DHCP network server, if you cannot connect your computer and
the SimpleSwitch™ device to a network supporting DHCP.
By default the container is not active, but is installed into all of our base images. See Base image downloads.
Registration
If you want to test SimpleCore™, SimpleSwitch™ or any of our packages from our SimpleCore™ incubator program, please register here and we will grant you access.
Not available for QEMU
As QEMU is already creating a local network to work with your device, this package is not
available for qemu86-64 MACHINE
Step-by-step instructions#
connect with a RS232 interface to your device
on your computer’s side use PuTTy or picocom to connect to the device (115200 Baud 8N1)
login with
rootrun
$ simpleswitch-helper start simpleswitch-dhcp-helper
connect an ethernet cable between your computer and
ETH0of the deviceyou should now receive an IP address from the device in the range
172.16.240.2-172.16.240.250To checkon Windows:
$ ipconfigfrom a cmd.exe terminal
on Linux:
$ ip a
from a terminal
you can now connect to
simpleswitch.local, e.g.$ ssh root@simpleswitch.local
and you can even use
simpleswitch.localinstead of an IP address for all the simpleswitch SDK tools
Note
The container will be again deactivated on a reboot. To permanently active the feature run
$ simpleswitch-helper enable simpleswitch-dhcp-helper
Advanced configuration#
In case the default settings would cause trouble with other networks your computer is connected to, you
can change the settings by creating on the device a file /apps/simpleswitch-dhcp-helper/config.conf:
NET_INTERFACE=ETH0
NET_NETWORK_PREFIX=172.16.240
NET_LEASE_TIME=10m
NET_INTERFACEis the name of the network interface DHCP support should be enabled onNET_NETWORK_PREFIXare the first 3 bytes of the IP range, your computer would get an IP assignede.g. with
NET_NETWORK_PREFIX=1.2.3your computer’s IP will be between1.2.3.2and1.2.3.250
NET_LEASE_TIMEis the time the IP assignment will be valid before an automated renewal