Getting started with Flutter#
Before you start#
Before we can use the SimpleSwitch™ SDK for Flutter we need to download the SDK extension. For this you need to run from the sourced SimpleSwitch™ SDK
$ GITHUB_TOKEN="<your personal access token for Github>" GITHUB_USERNAME="<your Github username>" simpleswitch-sdk-tool install flutter
$ eval "$(simpleswitch-sdk-tool activate)"
Github personal access token
To create a Github personal access token see Github container registry (GHCR)
Example Flutter Project#
To create an example project, you may use
$ flutter create myapp
myapp can be replaced by the name of your application.
Build the Flutter project using CLI#
In order to build and deploy using Flutter, you will need to add a Flutter custom device.
Adding a Flutter custom device#
A custom device can be added using the command flutter-add-simpleswitch-device coming with the SimpleSwitch™ SDK
$ flutter-add-simpleswitch-device <device_id> <target_ip>
Building and Running on custom device#
Using flutter command, you will be able to build and deploy the application
with a single command
$ flutter run -d <device_id>
Where <device_id> is the id you specified for your custom device in Flutter
configuration file.
If you want to build a package without deploying, please refer to Using an external tool section below.
Managing Flutter custom devices#
You can list existing custom devices
$ flutter custom-devices list
You can delete a specific custom device
$ flutter custom-devices delete -d <device_id>
To modify the configuration of an existing custom device, you can directly modify the custom devices configuration file in ${XDG_CONFIG_HOME}/.config/flutter/custom_devices.json. This can be useful to tweak the startup command, modify the install process, etc.
Using an external tool with Flutter#
You can also build from command line using flutter utility
$ flutter-create-bundle
You can then use the --copy-dir option of the
simpleswitch-generate-package the
Generate a SimpleSwitch™ package
$ simpleswitch-generate-package --name simpleswitch-example --copy-dir build:/usr/share/simpleswitch-example \
--template flutter --startup-command '/usr/bin/flutter-runner simpleswitch-example -f'
For a different than the release profile try
$ flutter-create-bundle --debug
$ simpleswitch-generate-package --name simpleswitch-example --copy-dir build:/usr/share/simpleswitch-example \
--template flutter --startup-command 'FLUTTER_MODE=debug /usr/bin/flutter-runner simpleswitch-example -f'
respectively
$ flutter-create-bundle --profile
$ simpleswitch-generate-package --name simpleswitch-example --copy-dir build:/usr/share/simpleswitch-example \
--template flutter --startup-command 'FLUTTER_MODE=profile /usr/bin/flutter-runner simpleswitch-example -f'
Debugging running Flutter application#
Before debugging a running application, you must get the observatory URI, exposed by Flutter on startup. This can be done using following command
$ ssh root@<target_ip> journalctl -u simpleswitch-app@simpleswitch-example.service | grep 'Observatory listening on'
Optionally, you can start the Flutter devtools, allowing to debug the running code
$ flutter pub global run devtools
Then, in your Flutter application source directory, you can then use a Flutter attach command
$ flutter pub get
$ flutter attach -d custom-devices --debug-url <observatory URI>
- Now you can interact as with an application running locally:
Modify the sources and use
Hot reloadwith therkey.If you started the devtools, use the live debugger. It’s URL should be printed in the console:
The Flutter DevTools debugger and profiler on imx8 is available at:.
Further reading#
See also