Getting started with C/C++#
If you want to create a SimpleSwitch™ application using C/C++, please follow this guide to get you easily started.
Example Project#
Here is a very small C project, with a single C source file, test.c:
// SPDX-FileCopyrightText: (C) 2022 Avnet Embedded GmbH
// SPDX-License-Identifier: LicenseRef-Avnet-OSS-1.0
#include <stdio.h>
int main()
{
while(1) {
fprintf(stderr, "Test C SDK\n");
sleep(5);
}
return 0;
}
And a Makefile:
# SPDX-FileCopyrightText: (C) 2022 Avnet Embedded GmbH
# SPDX-License-Identifier: LicenseRef-Avnet-OSS-1.0
BIN = c_test_prog
OBJS = test.o
all: $(BIN)
$(BIN): $(OBJS)
$(CC) -o $@ $<
clean:
rm -f $(BIN) $(OBJS)
install: $(BIN)
install -m 0755 -d "$(PREFIX)/opt/$(BIN)"
install -m 0755 $(BIN) "$(PREFIX)/opt/$(BIN)"
.PHONY: clean install
One can build this project for the host system by putting both file in the same
directory and running make
$ make
cc -c -o test.o test.c
cc -o c_test_prog test.o
$ ./c_test_prog
Test C SDK
Build the project using a Makefile#
With a makefile aware of cross-compilation, building the binary is as simple as
sourcing the SDK and running make, e.g.
$ . /opt/sc/0.1.0/sm2s-imx8plus/environment-setup-cortexa53-crypto-simplecoredistro-linux
$ make
aarch64-simplecore-distro-linux-gcc ... -o test.o test.c
aarch64-simplecore-distro-linux-gcc ... -o c_test_prog test.o
If the makefile has an install target using the PREFIX variable as
installation path, it can be used directly with the --makefile-dir option of
the Generate a SimpleSwitch™ package script
$ simpleswitch-generate-package --name simpleswitch-example --makefile-dir . \
--template C --startup-command /opt/c_test_prog/c_test_prog
Or if you want to be able to debug your application:
$ simpleswitch-generate-package --name simpleswitch-example --makefile-dir . \
--template C --startup-command "while true; do gdbserver :2159 /opt/c_test_prog/c_test_prog ; done"
If your makefile lack of a compatible install target, see below.
Build the project using an external tool#
You can also build with any external tool and create a package by copying the content of a directory. All you need is this directory to reproduce the structure desired in the package
$ find deploy_dir -printf "%y %p\n"
d deploy_dir
d deploy_dir/usr
d deploy_dir/opt/c_test_prog
f deploy_dir/opt/c_test_prog/c_test_prog
You can then use the --copy-dir option of the
simpleswitch-generate-package the
Generate a SimpleSwitch™ package
$ simpleswitch-generate-package --name simpleswitch-example --copy-dir deploy_dir \
--template C --startup-command /opt/c_test_prog/c_test_prog
Or if you want to be able to debug your application:
$ simpleswitch-generate-package --name simpleswitch-example --copy-dir deploy_dir \
--template C --startup-command "while true; do gdbserver :2159 /opt/c_test_prog/c_test_prog ; done"
Deploy to the target#
Now it is time to deploy the generated SimpleSwitch™ container to the device. For this please see Deploy a SimpleSwitch™ package
Remote debugging a C/C++ application#
To remote debugging a C or a C++ application, you can see Remote debug a SimpleSwitch™ package
Further reading#
See also